Skip to main content
Associate III
July 20, 2024
Question

FreeRTOS Code issue Data Sending on the server

  • July 20, 2024
  • 1 reply
  • 823 views

Hello 

I am working on the Free RTOS code that I am trying to send the data on the server using Free RTOS but I am not able to send data on the server I am using some dummy data and GPS for location +STM32F411ceu6a+EC200U GNSS. But my RTOS task is not working can some one plz help me find the problem in my code.

CODE:-

// Globals
QueueHandle_t xQueue;
SemaphoreHandle_t xBinarySemaphore;

typedef struct {
 float Latitude;
 float Longitude;
 float objectTemp;
 float ambientTemp;
 float xG;
 float yG;
 float zG;
 float avg;
} GPSData_t;


/* Definitions for ec200u6 */
osThreadId_t ec200u6Handle;
const osThreadAttr_t ec200u6_attributes = {
 .name = "ec200u6",
 .stack_size = 128* 4,
 .priority = (osPriority_t) osPriorityRealtime,
};
/* Definitions for L89 */
osThreadId_t L89Handle;
const osThreadAttr_t L89_attributes = {
 .name = "L89",
 .stack_size = 128 * 4,
 .priority = (osPriority_t) osPriorityRealtime,
};
/* Definitions for myQueue01 */
osMessageQueueId_t myQueue01Handle;
const osMessageQueueAttr_t myQueue01_attributes = {
 .name = "myQueue01"
};
/* Definitions for myMutex01 */
osMutexId_t myMutex01Handle;
const osMutexAttr_t myMutex01_attributes = {
 .name = "myMutex01"
};
/* Definitions for myBinarySem01 */
osSemaphoreId_t myBinarySem01Handle;
const osSemaphoreAttr_t myBinarySem01_attributes = {
 .name = "myBinarySem01"
};


void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_ADC1_Init(void);
static void MX_I2C1_Init(void);
static void MX_SPI1_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_USART6_UART_Init(void);
void Startec200u6(void *argument);
void StartL89(void *argument);


 // Create the queue
 xQueue = xQueueCreate(10, sizeof(GPSData_t)); // Adjust the size as needed

 // Create the binary semaphore
 xBinarySemaphore = xSemaphoreCreateBinary();

 if (xQueue != NULL && xBinarySemaphore != NULL)
 {
 // Create the tasks
 xTaskCreate(Startec200u6, "Task2", configMINIMAL_STACK_SIZE, NULL, 1, NULL);
 xTaskCreate(StartL89, "Task1", configMINIMAL_STACK_SIZE, NULL, 1, NULL);

 // Start the scheduler
 vTaskStartScheduler();
 }

 /* USER CODE END 2 */

 /* Init scheduler */
 osKernelInitialize();
 /* Create the mutex(es) */
 /* creation of myMutex01 */
 myMutex01Handle = osMutexNew(&myMutex01_attributes);

 /* USER CODE BEGIN RTOS_MUTEX */
 /* add mutexes, ... */
 /* USER CODE END RTOS_MUTEX */

 /* Create the semaphores(s) */
 /* creation of myBinarySem01 */
 myBinarySem01Handle = osSemaphoreNew(1, 1, &myBinarySem01_attributes);

 /* USER CODE BEGIN RTOS_SEMAPHORES */
 /* add semaphores, ... */
 /* USER CODE END RTOS_SEMAPHORES */

 /* USER CODE BEGIN RTOS_TIMERS */
 /* start timers, add new ones, ... */
 /* USER CODE END RTOS_TIMERS */

 /* Create the queue(s) */
 /* creation of myQueue01 */
 myQueue01Handle = osMessageQueueNew (16, sizeof(uint16_t), &myQueue01_attributes);

 /* USER CODE BEGIN RTOS_QUEUES */
 /* add queues, ... */
 /* USER CODE END RTOS_QUEUES */

 /* Create the thread(s) */
 /* creation of ec200u6 */
 ec200u6Handle = osThreadNew(Startec200u6, NULL, &ec200u6_attributes);

 /* creation of L89 */
 L89Handle = osThreadNew(StartL89, NULL, &L89_attributes);

 /* USER CODE BEGIN RTOS_THREADS */
 /* add threads, ... */
 /* USER CODE END RTOS_THREADS */

 /* USER CODE BEGIN RTOS_EVENTS */
 /* add events, ... */
 /* USER CODE END RTOS_EVENTS */
 vTaskStartScheduler();
 /* Start scheduler */
// osKernelStart();


void Startec200u6(void *pvParameters)
{
 /* USER CODE BEGIN 5 */
 /* Infinite loop */
 GPSData_t receivedData;
 int retryCount;
 const int maxRetries = 2;

 for (;;) // Infinite loop for the task
 {
 if (xSemaphoreTake(xBinarySemaphore, portMAX_DELAY) == pdTRUE)
 {
 if (xQueueReceive(xQueue, &receivedData, portMAX_DELAY) == pdPASS)
 {
 // Retry sending data up to maxRetries times
 retryCount = 0;
 while (!sendHTTP(receivedData.Latitude, receivedData.Longitude,
 receivedData.objectTemp, receivedData.ambientTemp,
 receivedData.xG, receivedData.yG, receivedData.zG,
 receivedData.avg))
 {
 vTaskDelay(pdMS_TO_TICKS(2000)); // Delay for 2000 ms
 if (retryCount < maxRetries)
 {
 retryCount++;
 }
 else
 {
 break;
 }
 }
 }
 }
 }
 /* USER CODE END 5 */
}

void StartL89(void *pvParameters)
{
 /* USER CODE BEGIN StartL89 */
 GPSData_t gpsData;

 for (;;) // Infinite loop for the task
 {
 // Receive data from UART
 HAL_UART_Receive(&huart2, (uint8_t *)Rxdata, 700, 5000);

 // Get location data
 get_location(&gpsData.Latitude, &gpsData.Longitude, 0);

 // Populate other sensor data
 gpsData.objectTemp = 25.0; // Predefined value for object temperature
 gpsData.ambientTemp = 24.0; // Predefined value for ambient temperature
 gpsData.xG = 0.1; // Predefined value for X-axis acceleration
 gpsData.yG = 0.2; // Predefined value for Y-axis acceleration
 gpsData.zG = 0.3; // Predefined value for Z-axis acceleration
 gpsData.avg = (gpsData.xG + gpsData.yG + gpsData.zG) / 3.0; // Calculate average
 // Toggle the pin to indicate data reception
 L89_TogglePin(2, 3);

 // Attempt to send the data to the queue
 if (xQueueSend(xQueue, &gpsData, portMAX_DELAY) != pdPASS)
 {
 // Handle queue send error
 }
 else
 {
 // Data was successfully queued, give the semaphore
 xSemaphoreGive(xBinarySemaphore);
 }
 }
 /* USER CODE END StartL89 */
}

 

This topic has been closed for replies.

1 reply

Pavel A.
July 20, 2024