cancel
Showing results for 
Search instead for 
Did you mean: 

Problem whit STM32F401RE as USB HID Device when using ADC

pablin235
Associate II

Hi, i'm using my Nucleo STM32F401RE as a HID Device for a MIDI Keyboard project

I have configured the following:

Connectivity --> USB_OTG_FS --> Device Only

Middleware --> USB_DEVICE --> Human Interface Device

I followed a video tutorial to configure the USB MIDI Descriptor in the file usbd_hid.c and it worked, my notebook detects my Nucleo as a USB Device and I have made a code to send only MIDI Note On and Note Off messages up to now, when pushing the Nucleo switch.

The problem comes when trying to use a potentiometer to send Control Change messages. I tried to use the ADC with interrupt and with DMA but when i use it, my notebook fails to detect the board as a USB

If i comment the line that initializes the ADC (HAL_ADC_Start_DMA) it works, but when uncommenting it again the ADC works fine but the HID doesn't

I'm not sure if i have an issue with the configuration of the ADC or USB or if maybe they are incompatible

The code in the main.c is the following:

 

 

 

 

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "usb_device.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "usbd_hid.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc1; DMA_HandleTypeDef hdma_adc1; /* USER CODE BEGIN PV */ extern USBD_HandleTypeDef hUsbDeviceFS; //MIDI Message arrays: 4 Bytes uint8_t midiNoteOn[4]; uint8_t midiNoteOff[4]; uint8_t botonEstadoActual = 0; uint8_t botonEstadoAnterior = 0; uint8_t botonTimeOut = 10; uint8_t lastDebounceTime = 0; uint8_t botonTimer = 0; uint16_t adc_val = 0; uint32_t buffer = 0; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_ADC1_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ //NOTE ON MESSAGE //Header Byte (Solo para MIDI USB) midiNoteOn[0] = 0x09; //Cable Number 0 (puede ser de 0 a F), el 9 es el Codigo (CIN) de NoteOn //Status Byte (El primer Nibble es el comando (NoteOn) y el segundo el Canal midiNoteOn[1] = 0x90; //9 es para NoteOn y 0 es el Canal 0 //Data Byte 1 --> Es el numero de nota, valor entre 0 y 127 pues el MSB de un data byte siempre es 0 midiNoteOn[2] = 0x40; //0x40 es 64 //Data Byte 2 --> Es la velocidad, la dejamos en un valor constante por no medirla midiNoteOn[3] = 0x7F; //0x7F es 127, ponemos el maximo //NOTE OFF MESSAGE //Header Byte (Solo para MIDI USB) midiNoteOff[0] = 0x08; //Cable Number 0 (puede ser de 0 a F), el 8 es el Codigo (CIN) de NoteOff //Status Byte (El primer Nibble es el comando (NoteOn) y el segundo el Canal midiNoteOff[1] = 0x80; //8 es para NoteOff y 0 es el Canal 0 //Data Byte 1 --> Es el numero de nota, valor entre 0 y 127 pues el MSB de un data byte siempre es 0 midiNoteOff[2] = 0x40; //0x40 es 64 //Data Byte 2 --> Es la velocidad, la dejamos en un valor constante por no medirla midiNoteOff[3] = 0x7F; //0x7F es 127, ponemos el maximo uint8_t retorno = 0; /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_USB_DEVICE_Init(); MX_ADC1_Init(); /* USER CODE BEGIN 2 */ HAL_ADC_Start_DMA(&hadc1, &buffer, 1); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ botonEstadoActual = HAL_GPIO_ReadPin(Boton_GPIO_Port, Boton_Pin); botonTimer = HAL_GetTick() - lastDebounceTime; if(botonTimer > botonTimeOut) { if(botonEstadoActual != botonEstadoAnterior) { lastDebounceTime = HAL_GetTick(); if(botonEstadoActual == 0) { //midiNoteOn[2] = (buffer*127)/4096; //midiNoteOff[2] = (buffer*127)/4096; while(((USBD_HID_HandleTypeDef *)hUsbDeviceFS.pClassData)->state==USBD_HID_BUSY) { } retorno = USBD_HID_SendReport(&hUsbDeviceFS,midiNoteOn,4); if(retorno == 0) HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET); } else { while(((USBD_HID_HandleTypeDef *)hUsbDeviceFS.pClassData)->state==USBD_HID_BUSY) { } retorno = USBD_HID_SendReport(&hUsbDeviceFS,midiNoteOff,4); if(retorno == 0) HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET); } botonEstadoAnterior = botonEstadoActual; } } } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 72; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4; RCC_OscInitStruct.PLL.PLLQ = 3; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief ADC1 Initialization Function * @PAram None * @retval None */ static void MX_ADC1_Init(void) { /* USER CODE BEGIN ADC1_Init 0 */ /* USER CODE END ADC1_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC1_Init 1 */ /* USER CODE END ADC1_Init 1 */ /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) */ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.ScanConvMode = ENABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 1; hadc1.Init.DMAContinuousRequests = ENABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); } /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. */ sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC1_Init 2 */ /* USER CODE END ADC1_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA2_CLK_ENABLE(); /* DMA interrupt init */ /* DMA2_Stream0_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn); } /** * @brief GPIO Initialization Function * @PAram None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : Boton_Pin */ GPIO_InitStruct.Pin = Boton_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(Boton_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : USART_TX_Pin USART_RX_Pin */ GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF7_USART2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : LD2_Pin */ GPIO_InitStruct.Pin = LD2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

 

 

 

I hope someone can give me a hand!

Thank you!

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

>  sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;

You're swamping the system with ADC interrupts so the USB doesn't have time to respond. Increase the sampling time to max and/or increase the number of samples you take before calling the ADC half/complete callbacks.

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

>  sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;

You're swamping the system with ADC interrupts so the USB doesn't have time to respond. Increase the sampling time to max and/or increase the number of samples you take before calling the ADC half/complete callbacks.

 

If you feel a post has answered your question, please click "Accept as Solution".

Hi TDK!

Thank you so much, it worked!

It's my first time working with USB so I wasn't aware that a high sampling frequency could affect the USB response

Greetings!