STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C integration using DMA Driver

Hi All,I am integrating the IMU sensor Using I2C DMA in circular mode on stm32f103c8t6 using Hal Library, so facing an issue reading the address value.In the below code "HAL_I2C_STATE_READY " this flag is not resetting after once function executes so...

Piyoosh by Associate III
  • 1271 Views
  • 2 replies
  • 0 kudos

Resolved! lwip on CM4 STM32h745

Hello,  I am trying to setup the CM4 core with lwip+mbedtls working. Actually I get this code working on CM7 but I need to migrate it to CM4. When I run the code the CM4 get a ard fault interrupt. Debuging I can see that this happens in HAL_MPU_Enabl...

RafaelS by Associate III
  • 1980 Views
  • 3 replies
  • 2 kudos

Resolved! How do I configure/program with MDMA?

Hi All,I am struggling with that the maximum DMA buffer size is 64KB. I am currently transferring the data from an ADC to the Buffer using DMA with circular buffering, but I would want the buffer to be around 200KB. I have heard that one can use MDMA...

elso by Senior
  • 4833 Views
  • 6 replies
  • 0 kudos