STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AN4457 UART Emulation - use via CubeMx?

Split from old (2020), abandoned thread: https://community.st.com/t5/stm32cubemx-mcus/uart-emulation-an4457-is-it-possible-to-use-it-via-cubemx/td-p/310812 for better visibility - and to enable marking a solution...Hi,I have the same problem, trying ...

JR72 by Associate
  • 930 Views
  • 2 replies
  • 2 kudos

Resolved! STM32F4 USBX CDC-ACM Bulk IN endpoint Stall

I am looking for help solving a CDC-ACM problem with Azure Rtos ThreadX, and the USBX Middleware for STM32F4.My device is an STM32F427VGTx.I currently have a project that uses the USBX host library. I am connecting up to 4x CDC-ACM devices through an...

akorsich by Associate II
  • 1470 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F0x0 custom bootloader

This is not a question, but a solution to a problem that took me forever to solve. This may be evident to many, but it was not to me, soI hope this will save others (and my future self) a lot of time...I was trying to implement a custom bootloader, w...

EvO by Associate II
  • 1171 Views
  • 1 replies
  • 4 kudos

Resolved! force input buffer for CRC to be aligned 32 bits

Dear ST community,I noticed that the CRC API is forcing the input buffer to be aligned 32 bits, which can be understood in order to be generic, but in the majority of the case we have a byte buffer which could be stored in unaligned in the memory or ...

Bassem by Associate II
  • 3303 Views
  • 7 replies
  • 5 kudos