STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5 sleep

hi all,i am developing a project using stm32u585 microcontroller which can connect to the external devices using ethernet and USB protocols.i need to put the controller in sleep or any low power mode when ever a sleep command is reached through the U...

sabari1 by Associate III
  • 3068 Views
  • 3 replies
  • 0 kudos

Resolved! Problem communicating with bootloader on STM32F7

Hello, I am trying to use one MCU to program another MCU, both of which are STM32 F746ZG boards.Let the MCU that is sending the commands be MCU 1, and the MCU in the bootloader mode be MCU2.I use the following command in the MCU2 to start its default...

is45_0-1750677679135.png
is45 by Associate III
  • 1102 Views
  • 4 replies
  • 5 kudos

Resolved! RTC Issue

Hello Community!I have an issue with reading / writing the RTC in an H723 MCU.The issue is:I can set the Clock to a date, but when I read out the RTC, then the year is 10 years in the future.e.g. I set the time to now (2025 / 06 / 22 19:mm:ss) and I ...

CBerg by Senior II
  • 1349 Views
  • 4 replies
  • 0 kudos

Resolved! HardFault Error in HAL_SD_Init()

Hi allI'm struggling for a while getting a µSD Card to run via SDMMC on FileX. I'm using a Nucleo U575 Board with an external SDMMC/SDIO-breakout board. I tried to follow the "Fx_uSD_File_Edit" example for the U575I-EV board.Long story short, I set u...

MGuth.1 by Associate III
  • 3208 Views
  • 8 replies
  • 0 kudos