User Activity

 I'd be glad to help you create a post about the Ethernet and LwIP implementation issues you're facing after following the article you linked. Here's a comprehensive response incorporating insights from potential causes and solutions, while adhering ...
 Hi STM32 Community,I am working on setting up bi-directional communication over FD CAN using the STM32CubeIDE with an STM32 micro controller (Nucleo-H753ZI). While I am successfully able to send data via the FD CAN TX interface and verify it on a CA...
Hi everyone, I'm working on a project using the Nucleo-G474RE board and the Arduino IDE. I'm aiming to utilize advanced peripherals like FDCAN and USB. While the Arduino Core for STM32 provides a simplified interface, I'm facing challenges in directl...
Hello ST Community,I am currently working on a project to design an Ethernet-to-CAN Gateway and implement Automotive Ethernet (SOME/IP) functionality over it. The objective is to enable seamless communication between CAN FD networks and Ethernet-base...
hi,    I'm new to STM32 and I need assistance with Ethernet configuration on the Nucleo-H7Z3G board. I'm starting from the beginning and hence I want to achieve the following: 1. Configuration of the Ethernet interface: RMII/MII on Nucleo-H7Z3G 2. Co...