STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HardFault Error in HAL_SD_Init()

Hi allI'm struggling for a while getting a µSD Card to run via SDMMC on FileX. I'm using a Nucleo U575 Board with an external SDMMC/SDIO-breakout board. I tried to follow the "Fx_uSD_File_Edit" example for the U575I-EV board.Long story short, I set u...

MGuth.1 by Associate III
  • 3228 Views
  • 8 replies
  • 0 kudos

Resolved! lwIP init sequence in STM32F439 Nucleo Cube

Hi,I have created an lwIP + FreeRTOS application using CubeIDE for my Nucleo 439 Board. The problem here is that the the init sequence generated by CubeIDE LWIP/App/lwip.c functionMX_LWIP_Init()it calls the following function without checking for the...

wrong_code.png avinash_elec_0-1750390963828.png

STM32H750-DK ETH issue

Hi Sir,       This is shiva chary ,am trying to implement Ethernet without LwIP,so when am configuring the ethernet MAC it is not resetting and am getting timeout error. can u please provide the solution for the respective errorThank youregards,shiva...

USB HS in STM32U5A5

Hello,We are thinking of switching from STM32F446 MCU to STM32U5A5 MCU in our device which is still in R&D.We are coding as bare metal. Since we are working with battery, low power is important for us. Also, our Quad SPI and USB HS work is critical a...

inancmert by Associate II
  • 1590 Views
  • 6 replies
  • 0 kudos

Read ADC from 2 joysticks with STM32F4xx

My project is a two-player Pong game using two joysticks, with each joystick controlling one paddle. The user interface was created using Touch GFX. The board is an STM32F429, and I have configured ADC1 to use channels 0 and 8. I’m using interrupts, ...

trungvan by Associate
  • 1085 Views
  • 5 replies
  • 1 kudos