Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello,I am currently using STM32N6657XOHXQ(Discovery Kit), I am running the (XSPI_NOR_MemoryMapped_DTR) example from STM32CubeMX. I have added UART print to debug the issue. Below are steps to reproduce the issue I am seeing.1. Put the board in devel...
need to know dev board for the STM32L552RET6TR. Also what is the specific part number used on this dev board.
STM32g474 code execute automatically without pressing RUN when i put MCU in debugging mode in uVision.Anyone knows where im wrong?Note:- Reset pin is not connected pull up or down.
Hello everyone,I am currently working on interfacing the Winbond W25Q16JV with my STM32H745 custom board over QSPI but have been facing issues with communication. I've utilized resources from ST’s QSPI library available at:ST QSPI DriversDespite foll...
Anyone have any experience with BGA hand soldering? I have always tried to stay away from BGA parts as far as prototyping and being able to rework a pcb. But now with choices between small pitch LQFP parts and BGA I am wondering if a 176 - 206 bal...
Hello,I am trying flash my STM32F746G Discovery board with new code from Linux. I run into this issue after running "dmesg -w": "can't set config #1, error -32". ST-Link is not being detected by either STMCubeIDE and STMCubeProgrammer. Has anyone run...
Hello, I‘m creating a counter that increments/decrements according to cw/ccw direction of an encoder. An interrupt is triggered by the rising and falling edge on each channel. Due to mechanical jitter, the interrupts are triggered (sometimes) simulta...
New question from this thread. So in order to use both SMPS and LDO, given in board schematics,I mounted SB6 and SB17 (SB44, SB46, L4 already mounted)and removed SB5 and SB18 (rest already not mounted).After than i flashed it with keeping the followi...
STM32H70-DK FDCANHello everyone:I want to use FDCAN in my board but it is not working.I've been using a few examples I've found as reference but none of them are for my exact board (STM32 H735).Does anyone have an example I can run?
Hello, Where to buy the cap of the Stm32H747-DISCO joystick, please kindly help. Thanks