Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, My board is acting strange. - When I use the USB to power the board (jumper JP3 on U5V) the led LD5 turns red ( the board draws more than 500mA). So I power the board with external power supply (5V and JP3 on E5V) but even if i'm able to flash th...
Hello, I have designed a circuit using the STM32F747XIH6, but I am unable to connect and flash the code using ST-Link. I have checked all the connections, and the NRST pin has a pull-up resistor and measures 3.3V. The 25MHz clock signal appears corre...
I just received a NUCLEO-H503RB dev board, and while attempting to use the GPIO_IOToggle example program to test out the board, I could not run the debugger due to the error "ST-Link not detected." I went back to my NUCLEO-H7S3L8 board, it now receiv...
I'm using an ST-Link V2 to stream (over ITM) code coverage data from an STM32G4 via GDB Server on a PC.This works fine most of the time (for many days), but the data stream sometimes drops some of the data. Adding a delay between calls to ITM_SendCha...
Hello, Im looking forward to get started with STM32 MCUs, planning to begin with a Discovery kit. Have few questions, before I get going.- Kindly suggest a Discovery kit, which has been there for sometime and is general purpose.- For code deve...
Hello all, How can I make a vias for the WLCSP156 to connect my internal layers from my PCB with WLCSP156 pads? If the pad diameter is only 0.220 mm in WLCSP156 , and the minimum hole for the vias at the factories is 0.15 mm (with ring is 0.25 mm tha...
I have an STM32 Nucleo-F446RE, which comes with an integrated ST-LINK/V2-1 debugger. I would like to use this ST-LINK to program an external STM32 MCU that does not have a development board.I checked the Nucleo schematics, and I see that ST-LINK/V2-1...
I'm using the STM32H753ZI Nucleo board with USB_OTG_FS communication,and I have enabled VBUS_SENSING. I would like to detect when the physical connection is lost,but I am not sure how to do it.Could you kindly provide any reference materials or guid...
looking to learn VFD is there any development boards related to VFD
I recently bought a Blue Pill, STLINK-V3MINIE and an adapter. How do I connect them together correctly?