User Activity

Hi all.I am confused about how I am supposed to provide power to the STM32MP257F-DK as it seems I am not providing enough power to the board when connecting the board to my PC via the STLINK/Power connector as the red Power LED is on and the Green LE...
Hi all, having an issue with programming STM32MP257F-DK/SDCard with the Starter package getting to the stage in the attached screenshot then it seems a connection times out with no success notification popup ?
Hi,Is there a guide out there to get a serial terminal set up with the STLinux "Starter" package on the STM32MP257F-DK up and running ? i.e what settings to use to connect, any needed hardware/connections/cables etc ?
Hello, at a glance the 40 Pin GPIO on the STM32MP257F-DK appears to be matching the Raspberry Pi standard, is this correct ? 
Hello,Would the B‑LCDAD‑HDMI1 adapter board work "out of the box" to connect a HDMI display to the STM32MP257F-EV1 running STM32MP2Starter ?
Kudos from