Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
hello ST Community,There's an STM32 board in a USB pen drive format with a small flash memory capacity and only a few pins (3-5 pins) for UART serial communication. On this STM32 board, inside the USB pen drive, I can program the dedicated software f...
Hello i'm new to STM32, i'm doing school project on in. Basically the plan is to read oil temperature from CAN bus in car, and display the temperature on analog clock using servo. I have the H755ZI-Q board for this. I know it's bit overkill for what ...
Hello,I am working with an STM32F103RB Nucleo board. I am able to successfully connect and program the device using ST-LINK, but I am facing an issue during debugging.The code is downloaded successfully and verified, but when the debugger tries to ru...
Hello I've been using a STM32L073RZ-Nucleo with a X-NUCLEO-IOD02A1 to test some functions and it works great. But the thing I'm wondering is if its possible to also add X-NUCLEO-PLC01A1 expansion board while using X-NUCLEO-IOD02A1 at the same time. ...
Hello,I am currently working on a schematic featuring 3x STM32H753ZIT6 MCU , and I have a few questions regarding the JTAG implementation:(1) From what I’ve gathered from various sources, the NJTRST signal is a JTAG ENABLE, meaning that in normal op...
Hello, I have 2 boards an STM32F407 disco and an STM3F746DISCO and i want to create a project that implements an external LCD screen to the board however when the project runned well with the F746 the screen didnt work with the F407 any guidelines?
Hello,I've just received my fresh new SMT32H747I-DISCO dev board and I wanted to try some samples.I have some experience deveolping on embedded Liuxes, but this is my second MCU (the first one was a Raspberry PICO, don't know if this counts). I am us...
I have this Riverdi board with a STM32H757XIH6 microcontroller. I have been using it consistently and loading touchgfx programs on it. Today I was trying to use the 40 pin header and program one of the gpio pins on it to act as a gpio output. I put ...
Hello, While using the Nucleo-F446ZE, I observed that pin PA1 remains at approximately 2.6 V during reset, even when an external pull-down resistor is applied. On this development board, PA1 can be configured as the RMII Reference Clock. However, I...
Hi, I would like to know when samples and kits for the new STM32H5E4/5E5 will be available.I already asked my local distributor this question, but they didn't know the answer. Ari