User Activity

Hi,I have developed an application using the STM32F103C8T6 MCU to function as a USB keyboard. The application uses the USB communication protocol to send keystrokes. One of the requirements is an emergency button that, when pressed, disables all othe...
Hi,I have developed a Keyboard using USB communication protocol and i am facing an issue, when i want to debug the code and parallelly i want to see whether the alphabet is printing or not. This is not happening when i want to see both simultaneously...
Hi,while connecting the stm32 blue pill board, the ST link(Debugger) is not detecting. And throwing an error, Failed to bind to port 61235, error code -1: No errorFailure starting SWV server on TCP port: 61235Failed to bind to port 61234, error code ...
Hi,please anyone could help me out how to resolve the issue regarding the ST-link upgrade. when i am trying to upgrade it is throwing an error "ST-link not in DFU mode. please restart it".I am facing this issue after updating both STM32cube IDE and S...
Kudos given to