cancel
Showing results for 
Search instead for 
Did you mean: 

Debug using ST-LINK USB Type-C on NUCLEO-N657X0-Q

qmarecat
Associate

Dear all,

I try to use ST-LINK USB Type-C to debog in CubeIDE IDE, however I have such error on CubeProgrammer by connecting the ST-link (see Picture 1). In CubeIDE, i have a different error (see Picture 2). The Nucleo is configured according to the default configuration in the documentation (jumper on BOOT0, BOOT1 & 1-2 to CN9)

Sincerely,

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @qmarecat and welcome to the Community,

Could you specify the version of STM32CubeProgrammer ? 

I recommend you follow these guides for debugging:

You can also refer to the videos about advanced debugging with CubeIDE: STM32CubeIDE Advanced Debug Features.

 

 
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @qmarecat and welcome to the Community,

Could you specify the version of STM32CubeProgrammer ? 

I recommend you follow these guides for debugging:

You can also refer to the videos about advanced debugging with CubeIDE: STM32CubeIDE Advanced Debug Features.

 

 
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
qmarecat
Associate

Dear Imen,

thank you for your Answer, 

I found how to do by switching up the BOOT1 jumper to 1 instead of 0.

Sincerely