Skip to main content
akif
Associate
May 7, 2020 10:21 PM UTC
Question

How to program a STM32 mcu without target power?

Hello,

I am looking for any programmer which programs the STM32 MCUs with the power of programmer.

So I don't want to connect any power to my MCU while programming it.

Is there any programmer like above?

Thanks.

#StayHomeBeSafe:D

This topic has been closed for replies.

2 replies

TDK
May 7, 2020 10:33 PM UTC

You can’t program a chip that isn’t powered. How would the flash operate?

There are knock off programmers out there that can supply power while programming.

"If you feel a post has answered your question, please click ""Accept as Solution""."
S.Ma
Principal
May 8, 2020 1:59 AM UTC

it is a power budget challenge.

if you want programmer to feed power, its power source and regulator shall be good enough, or its regulator might overheat.

if the programmer uses usb as power, usb devices have typically 100 up to 500mA total budget in usb 2.0 style.

did you consider these aspects?