cancel
Showing results for 
Search instead for 
Did you mean: 

No device found on target. ?

simo zz
Senior II

Hello,

After copying an STM32CubeIDe project using the New → Project from .ioc file and then importing old project version into the one, the IDE wont let me program the device.

With old project version, I can run the programming Run settings and the STLinkV2 reflashes the MCU.

With the new project version, STLink cannot find the device.

The Run settings are the same...

Any suggestion ?

Thanks.

s.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
simo zz
Senior II

Solved. Debug Runs must be set as well, not only the 'Release' one.

View solution in original post

1 REPLY 1
simo zz
Senior II

Solved. Debug Runs must be set as well, not only the 'Release' one.