STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L073RZT6 Hardware issue

Hello everyone,I am working on STM32L073RZT6 microcontroller and I have designed my custom board using this mcu. I am facing issue related to reset. The microcontroller is getting rest automatically however the period is not fixed.I understand the po...

0693W00000AN581QAD.png 0693W00000AN57NQAT.jpg
ABane.2 by Associate
  • 1359 Views
  • 0 replies
  • 0 kudos

Resolved! No ST-LINK detected! - Nucleo H723ZG

Hi,So far I was using Nucleo WB55 and everything was ok with ST-LINK. Now I created new project and switched to Nucleo H723ZG. When I try to run or debug I receive message:No ST-LINK detected! Please connect ST-LINK and restart the debug session.The ...

0693W00000AMjfcQAD.png 0693W00000AMjfhQAD.png
DPiór.1 by Associate III
  • 7443 Views
  • 6 replies
  • 0 kudos

Clock source selection for stm32f767

I am planning to use stm32f767 mcu. I am confused to use clock for the same. I am referring discovery board schematic but in that NZ2520SB-25.00M is used for MCU and Ethernet controller. In my case i won't be using ethernet. I will be using TFT inter...

SS.Sagar by Associate III
  • 2074 Views
  • 1 replies
  • 0 kudos

Hello, I have a wired mouse connected to STM32F407 discovery board and i followed your steps in the tutorial but it did not work. Could you please let me know what is the hardware connection required to achieve this setup?

Should pin PA9 needs to be connected to something on the board and is there any way to call the eventcallback function.My main issue is that the wired mouse is not asensed by Vbus.Its voltage is 0V. Could you please help me on this.Any help would be ...

SShub.1 by Associate II
  • 2009 Views
  • 3 replies
  • 0 kudos