Skip to main content
DonPavlov
Associate II
July 1, 2020
Question

ST-Link and STM3210E-EVAL

  • July 1, 2020
  • 2 replies
  • 691 views

I want to get an STM3210E-EVAL Board. It is mentioned in the eval board overview that the used stlink is ST-Link V3/E. But in the ressources i cant find any reference to it.

Do i need to buy an ST-Link V3/E to debug the Hardware, or is the ST-Link onboard like the nucleo versions?

Also the new ST-Link V3 is modular. Would i need specific modules?

Fast Help appreciated

This topic has been closed for replies.

2 replies

Uwe Bonnes
Chief
July 1, 2020

STM3210E-EVAL does not have a built-in STlink. JTAG/SWD is available as 2 20 Pin connector . Stlinkv3 and Stlinkv2 have the corresponding connector, as does a JLINK and many other debuggers.

DonPavlov
DonPavlovAuthor
Associate II
July 3, 2020

But why does it mention STLink V3E here :

STM32-Eval-Boards

For me it is just a question of do i need an extra Debugger or not. A JTAG 20 Pin port is there so i can easily use it.