Hi, i am using st link v3. with stm32 cube programmer v2.4.0.hardware = stm32L071set the RDP level to AA.i can write the eeprom only once on same address, if i try to change the value on same address then cube programmer is block. please take look on...
Packages DetailsSTM32F446RE NucleoCubeMX 5.6.0STM32CubeF4 Firmware Package V1.25.0 / 12-February-2020if i write every 30ms 512 Bytes. After some time SD card takes more time then normal please check image.GPIO Pin Set before writing and Reset after w...
HI, I am using windows 10 with visual Studio 2017. Stm32CubeProgrammer V2.3.0. I like to use the CubeProgrammer_API.lib in my custom project. one thing which is not clear to me. what is the purpose of "STM32_Prog_DB.xml" file. Visual Studio ...
Hello. i am using stm32L0 family.i have ST-Link V3. its working fine with st link utility tool. i can connect using cli command with normal mode. so the issue is Connect under Reset. CLI command is not working if i connect in Connect under Re...
Hi. is there any example using 902 – 928 MHz just using S2LP(no Sigfox), which fulfill the FFC standards regarding to the frequency hopping. according to AN4949, my understanding , in SRadioInit base frequency would be 902 Mhz with frequency de...
thank you for quick reply. there is no option in cubeprogrammer to erase the eeprom memory. if i try to write Zeros(0) inside cell before rewriting, still this is also not working.here is log form rewirting. cube pro is trying to erase but not succes...
@Nesrine.JLASSI short feed back from side. stm32L07x family is working fine.when i test with stm32L051.i have same issue.St link V3Cube programmer V2.4connect under reset.here is error msg from cubeprogrammer "Error: ST-LINK error (DEV_CONNECT_ERR)"...
Posted on March 19, 2016 at 20:57i am also working on L6480 Stepper motor Driver.i also follow the diagram from the eve board.so now i am getting confuse.do i need to follow your diagram or orginal means eve board diagram.i hope St support will give...