STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401: Voltage dependence of RAM

Hello,I am developing a bootloader that is entirely executed from RAM. If I run the code from a Nuceleo board the MCU is supplied with 3.3V, program executed fine. If i go to target hardware (which runs on 2.5V!!), the cycle speed is reduced by ~14%....

LGrüb.1 by Associate III
  • 1519 Views
  • 2 replies
  • 0 kudos

Resolved! Why does ST-Link Server not start properly?

Hi!I recently tried to put my Nucleo G071RB board back in use.Sadly it refused to work.I´m using Cube IDE, Windows 10 (64).After some research I found out, that Cube IDE is using ST-Link Server software to connect to the board, of which I installed t...

PHirs.1 by Associate II
  • 3735 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L4P part longevity/lifetime

I'm considering using a STM32L4P in a medical device design. What is this part's expected longevity in the market. Will I still be able to buy it in 5 or 10 years?Do any ST processors have a guaranteed product lifetime?