Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello Im using STM32F303K8T6 controller...Im flashing my code from keil using ST-Link...I can't put my controller in debug mode...It directly goes to run mode...hardware reset is also not working... please help me
download errorr via swd mode
Where can I find the datasheet for the IEG1120TB103GF-001 display on my 32L4R9IDISCOVERY? The only Google result shows a PDF that doesn't include the startup sequence, and the demo code has what seems to be completely arbitrary initialization sequenc...
Hello! The problem is ST-Link V3 not always connect to the target with ST-Link GDB Server. It can connect one time, but next ten times doesn't connect. Reboot the programmer or reboot target doesn't help. With OpenOCD - works great with the same cabe...
Hi All,My board is built on the STM32F746IG.Some time after the launch of the firmware (3 different firmware) access via SWD is unavailable.Stm32_Link_Utility reports:- Core is held in reset- Can not connect to target!..........Vnrst = 0.3 V, despite...
Hello!For a redesign of an already existing product we're using an STM32H743XI, which is a TFBGA240+25.The BGA balls "B6" and "F2" are documented in two different ways in the datasheet and in CubeMX, see also attached picture.Datasheet "DS12110" (ver...
Hi, I would like to use the STM32F746G-DISCO to do a project. But the pins available on it are quite few (only PA0-PA5 and PD0-PD15). I wonder if those pins' function are fixed because I only succeeded to use PA0 as PWM Output of TIM5. It seems like...
Hello,i am using the ST-LINK Utility 'Serial Wire Viewer' for debbuging three MCU, which are communicating to each other. For a fast opening and exact placement of the windows i use my autohotkey script. Everything work fine, but now i want to set th...
The schematic and insert card disagree.The VCP is USART3 PB10/PB11 (verified)The Arduino header D0/D1 is PB7/PB6 USART1UM2488 described in the data brief is also missinghttps://www.st.com/resource/en/user_manual/DM00547983.pdfhttps://www.st.com/resou...