Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello,I want to use the board with STM32F407VET6 processor. But when debugging, it gives a "No ST-LINK detected" error. Also, I downloaded the ST-LINK Utility and when I press the CONNECT button, I see the same error "No ST-LINK detected". It shows a...
Total power consumption at 5 Volt (external) input
to start, i would like to say that i was taking Udemy Course related to Embedded C - Absolute Beginners. in the tutorial it was not clearly explain how to port the STM32 and connect it to IDE. this are the chronological order:i first i try to install...
I am working on a schole projekt and there I neded to design a PCB that can talk to the PC over USB. whiel doing that I am not able to figure aout whie the USB connection dous not work if it is not set for programming.In detail:The USB Connection is ...
Could anyone point me to a good description of the Mbed firmware update feature of ST-LINK, via "USB disk"?What image formats does it accept?Can it load (and run) images located in internal RAM?
I'm learning how to make a PCB with an STM32H725IGK6 MCU (UFBGA), which will be used as a flight controller for a drone. This is the first proper attempt I've done at creating a schematic, so I would appreciate it if someone more experienced would be...
I don't know what to do, sometimes when it installed and i tried to open it, it's show's that some files are missing?
IS STM32H750 TFBGA240 PIN TO PIN Compatible to replace with STM32H755 TFBGA240
https://www.st.com/resource/en/user_manual/um2488-discovery-kits-with-stm32h745xi-and-stm32h750xb-mcus-stmicroelectronics.pdfIn the pin list fails to identify the QSPI NCS pin candidates, I had to review schematicPG6 QSPI_BK1_NCS, PC11 QSPI_BK2_NCS /...