Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I am moving a smt32H750 application from flash to ram. In flash the st-link v3 works fine both single step and break points, but when moved to ram, it is diffucult to get the ST-LINK breaking the program. If the main-loop is extended (cache not cover...
For my project, i need to power a relay that works on 5V. But the outpout available to me from the board is only 3.3V and due to which it is not enough to power on the relay.There is a D5V pin on the CN6 connectors, but it does not give out 5V. do i ...
I bought a STM32H747i-DISCO board to learning USB HOST to drive a camera, I found the usb host is very unstable, every is fine except suddenly dropout which meanings the port disabled, I debug and struggle for months with no nothing solved. the USB...
I own a proprietary design based on STM32H743ZGT6.Two boards were assembled.Initially both boards work identically.After about two days of software bring-up activity on one board following issues were encountered:1) Debug through JTAG is not possible...
I was trying out various security protection mechanisms on my NUCLEO-H753ZI and after configuring the secure user memory area, I can no more access my STM32 via ST-LINK.I haven't configured the RDP, it was at L0. No other protections were set.I think...
Hello,I've reported my problem with ST-Link GDB server here:https://community.st.com/s/question/0D53W00002BBBlsSAH/stm32cubeide-debugging-issues-of-code-placed-in-sram-stm32h7-mcubut thread evolves and it more and more look like a real bug in ST-Link...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.