Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I'd like to build my own development board for learning purposes and I found a circuit on the Internet without much explanation. I want to solder this board but I have some concerns. My main questions are: Will this development board work?How can I p...
I have a custom board on which there is an STM32 microcontroller. The board doesn't include the ST-LINK so I bought it and connected it to the board for the debug. After that my pc cannot detect the COM port anymore. Somebody can help me? Thanks
I do not have room on my board for a large connector, so I need to create a custom cable. The STM32l010F4 boots via USART, yet I cannot find anything in the ST-link docs that says "connect this pin to usart Tx, and this one to the usart rx, etc.If so...
I am facing a problem while programming a board the arduino ide is unable to Detect the board and giving this error.and my Arduino ide Board Configuration areBut in Device Manager it detecting problem as shown below.and my board configuration are as ...
I am moving a smt32H750 application from flash to ram. In flash the st-link v3 works fine both single step and break points, but when moved to ram, it is diffucult to get the ST-LINK breaking the program. If the main-loop is extended (cache not cover...
For my project, i need to power a relay that works on 5V. But the outpout available to me from the board is only 3.3V and due to which it is not enough to power on the relay.There is a D5V pin on the CN6 connectors, but it does not give out 5V. do i ...