STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not able to debug with STM32F07 dev board. Attached the debug log, kindly help me in this. Thank

STMicroelectronics ST-LINK GDB server. Version 7.3.0Copyright (c) 2023, STMicroelectronics. All rights reserved.Starting server with the following options:    Persistent Mode      : Disabled    LogFile Name        : C:\Workspace\RTOS_Workspace\001_Ta...

SNaga.6 by Associate II
  • 4163 Views
  • 7 replies
  • 0 kudos

Resolved! Power Supply for STM32F4 Board via USB Vbus

Hi! I am working currently on a stm32 F407, I am implementing USB Communication Device Class with the microcontroller being a device. The microcontroller is powered via the STLink but I wanted to change that and supply it through the usb I am using f...

LimoGr by Associate II
  • 4626 Views
  • 1 replies
  • 0 kudos

Resolved! I made a prototype board using STM32H7A3LIH6Q. Before the firmware was written, a current of 500mA flowed(@+3.3V).

I made a prototype board using STM32H7A3LIH6Q.Before the firmware was written, a current of 500mA flowed(@+3.3V).VDD and VSS were not shorted.​Q1)Have there been such cases in the past?Q2)Are there any mistakes in the wiring of the circuit?Q3)VFBSMPS...

DE.1 by Associate II
  • 5542 Views
  • 8 replies
  • 0 kudos