STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7S7L8H6 SMPS mode

Hello Team,We are developing our new project by using STM32H7S7L8H6. We want to use STM32H7S7L8H6 in SMPS mode. So, refer attached schematic design image with SMPS mode. Request you to please review it and provide your valuable inputs.Note : In our a...

JK1234_0-1767071996188.png JK1234_1-1767072030005.png JK1234_2-1767072054305.png
JK1234 by Associate III
  • 445 Views
  • 2 replies
  • 1 kudos

Resolved! Is this a genuine ST-Link?

Originally a comment on the How to recognize a genuine ST-LINK/V2 versus a cloned one Knowledge Base article.Moved to main forum for better visibility / discussion.I bought this  ST-LINK V2 on Amazon ( see pictures) . I don't think its' a genuine STM...

20251230-090308.jpg 20251230-090300.jpg 20251230-090028.jpg 20251231-120348.jpg

Resolved! STLINK-V3-MINIE UART weirdness

Hello all and happy holidays, I am having a bit of weirdness going on. I have setup UART using stm32 HAL, confirmed it is working properly by stepping through (using an STLINK-V3-MINIE) as well as confirmed data is on the wire with a logic analyzer a...

Ruggs by Associate II
  • 700 Views
  • 6 replies
  • 3 kudos

No device found on target

Hi, I mistakenly used the pin for swd on my F446RE for other purposes and now it does not connect through st link.Can anyone guide me through a solution for it? The only thing I can do now is update the board. The two leds are always red.

Resolved! stm32n657-dk evb with spi interface

Hi Team, Currently, I am working on the STM32N657-DK EVB with an SPI interface (ADS118 sensor). I have enabled SPI5 in the .ioc file. The configured pins are: PE11 – SCK PH8 – MISO PG2 – MOSI PA3 – CS According to the schematic, these pins are c...

Kumar123 by Associate III
  • 553 Views
  • 1 replies
  • 1 kudos