cancel
Showing results for 
Search instead for 
Did you mean: 

Mic Interface Options on STM32H757I-EVAL

priya_12
Associate II

Can the STM32H757I-EVAL board accept microphone output in formats other than DFSDM or PDM? 

3 REPLIES 3
AScha.3
Super User

You can use any free (!) I2S or SAI input, to connect an I2S mic.

If you feel a post has answered your question, please click "Accept as Solution".
priya_12
Associate II

Thanks, how many external microphones can the board support? Is there any way that I can interface other microphones apart from st microphone in the board?

See circuit of eval board :

https://www.st.com/resource/en/schematic_pack/mb1246-h757-e02_schematic.pdf

Which pins on H757 are free and on which pins you can set I2S or SAI (in I2S mode) you can see....

respectively puzzle together from ds , pins, and circuit, whats free and on a header.

Or use Cube, to show what I2S or SAI are still free, to use by your new mic I2S .

If you feel a post has answered your question, please click "Accept as Solution".