Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, Is there an official source listing all evaluation, discovery, or development boards based on STM32H5 MCUs? Thanks,Aymen
Greetings, I know how to solve it , but I do want to reseach on this issue. I use a nucleo's stlink (nucleo F070RB) to program a stm32g030k8tx. However, the target is only detected and, therefore programmed, when the external mcu is not on standby mo...
Is there ST-Link V2 driver for Windows 11? I am using Microsoft Surface Pro + Copilot and trying to load code on STM32L476.
hey all, i'm working on a team where most people have little experience with stm32s, and we've designed and manufactured our first board with the STM32H7S3I8T6 chip. we followed the data sheet extensively and did a decent amount of research on periph...
I have an STM32H747I-DISCO board that I am trying to bring up with the Tutti Frutti Demo. I have followed the instructions in UM3008 to program this as it appeared to be blank upon arrival from Digikey. External loader was set to: MT25TL01G_STM...
I have managed to create a template application on a NUCLEO-H755 that has several CM7 FreeRTOS tasks running to flash various LED patterns combined with a CM4 application that flashes one of the other LEDs. I have mainly been testing using a run con...
Has anyone been able to get DAC2 Channel 1 on the NUCLEO-H7A3ZI-Q board to work at all? For anything? With DMA?
I'm using the STM32H747 DCMI peripheral to capture video from an OV5640 camera, and I've encountered a confusing situation regarding synchronization signal polarity.Development EnvironmentBoard: STM32H747I-DISCOCamera Module: B-CAMS-OMV (OV5640)Firmw...
Hi, I am working on the STM32N6570-DK board using the Load & Run boot mode.XSPI2 is used to interface the external flash (boot device).XSPI1 is used to interface an external PSRAM.The FSBL is loaded by BootROM and runs from internal SRAM.The FSBL ini...
Split from old thread Nucleo-H755ZI-Q How can I resolve ST-Link "No device found on target" error? - which is solved.i am using same mcu i have this error in the begining like target dectection now that target is dectecing problem is resolved but no...