STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5A9J-DK ITM

Hallo,is there something I have to check if ITM_SendChar doesn't work? I mean, I have overwritten the write function in syscalls.c and enabled in the debugger settings the swv viewer at the correct clock, enabled swv trace (the same things I did usin...

IVent.1 by Senior
  • 1442 Views
  • 1 replies
  • 0 kudos

USB Detection to Reprogram Nucleo Board

Hello,I have programmed a Nucleo-L476RG with the Blinking LED example. Until there is all fine.Now, I want to load a new program on the board. Windows Explorer and ST-Link do not detect the board and cannot load a new program on the board.I bought th...

Node.PNG
Rico1234 by Associate II
  • 1942 Views
  • 2 replies
  • 0 kudos

Nucleo-G031K8 Bricked

 My Nucleo-G031K8 can no longer be programmed using STM32CubeProgrammer or from STM32CubeIDE.  When attempting to connect using STM32CubeProgrammer I receive the following text:    UR connection mode is defined with the HWrst reset mode    Error: Est...

Resolved! LwIP Server

I am using a STM32H743 processor and have ST's LwIP stack running correctly. At least to the point were I can use Hercules as a client and connect to the Nucleo and send a small block of data (24 bytes) to the Nucleo. I have set breakpoints in the co...

GilRoss by Associate II
  • 4151 Views
  • 2 replies
  • 0 kudos

Resolved! Very silly problem (STM32F746G discovery board)

Hi everyone,I just picked up a STM32F746G discovery board to practice on, but I can't for the life of me get the built-in STLink to show in windows. By this I mean, I'm unable to power via mini-B and LD7 just flashes red. Once I change the jumper on ...

DevOne by Associate II
  • 4101 Views
  • 7 replies
  • 0 kudos