Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
programmed in IAR, for debugging im using stm32-utility,in this when i try to connect the target it shows can not connect to the target.What i did in this is 1.connected the jtag pins with respective.2.power supply 3.3v3.NRST is high4.BOOT0 is high
I erased on board stlink firmware by mistake.I got STLinkV2.J16.S4 bin file from a web site . and downloaded it into on board stlink with STM32 ST-LINK Utility.and then upgraded STLinkV2.J34.S4 to on board stlink by using ST-LinkUpgrade tool but L475...
Hi, I'm using the STM32F334K8T6 andI'm using EAGLE 9 to create PCBs.https://www.digikey.com/product-detail/en/STM32F334K8T6/497-14953-5-ND/4989175?WT.z_slp_buy=stm_stm32f3Does ST provide PCB libraries which I can use on EAGLE?Where can I get them?Sin...
Information about my computer, No St-Link device detectWhy.
Hi all, for those who are trying to use an external power supply on the STM32F746G-DISCO, yesterday we found that on the two cards we are using for our development, the solder on JP2 connector creates a shortcut... preventing the card to be used tha...
i'm using IAR embedded workbench and stm32f4 discovery board and j-link.i wanna try download application via SWD (J-Link) connection. So, first i remove CN3 jumper. and soldering resistor R2.but still can't download application. (IAR and st-link is ...
Hi,Is it possible to get Eagle schematics files for the DISCOVERY_STM32F429I, DISCOVERY_STM32F469I and the STM32_Nucleo-F429ZI ?Alternatively and export from Altium to ACCEL ASCII format would be fine.Or does anyone know of a way to convert Altium to...
Hello,I'm working for the first time with an ST-LINK V2 on a Windows 10 laptop, and it doesn't work with an MCU or without it.I am trying to isolate a problem, so I connecteed the ST-LINK on its own, without any attached wires, besides the USB that c...
When I try to connect to the board from CubeIDE I always get an error message. At first I was lacking GLIBCXX_3.4.2, but now that it has been installed, it still cannot connect.If I use STM32CubeProgrammer, I can read and write to the board withou is...