cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link/V2 ISOL can't connect after FW update

afla03
Associate

Hello,

I was using my ST-Link/V2 ISOL, to reflash some units, but after an update with the ST link updater my programmer suddenly not recognize the target board.

I tried to reflash with different versions but it says that is corrupted. Is the ST link updater the same for all the st link programmers?

Thank you!

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

I actually have 2 other ST link V2 and the connections are exactly the same, I am able to program the boards with the other 2.

Pavel A.
Super User

Yes the st-link updater is one for all variants. Try the latest version, on a good computer (with *supported* Windows or Linux) and good cables.

Do not change other options (if shown): clock, mass storage drive, etc.

Peter BENSCH
ST Employee

If the problem still exists: Can you please upload a photo of the ST-LINK/V2 ISOL and mark the faulty one there?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.