STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART1 and USART2 STM32H7B3I-DK

Hello everyone!I am working with STM32H7B3I-DK and I have enabled USART1 based on the available example, but I need to enable USART2 to connect to the WiFi. If I use the same code but with RX and TX pins from USART2, I can see nothing on console. Do ...

User1340 by Associate II
  • 4979 Views
  • 9 replies
  • 2 kudos

Resolved! stm32l073rz nucleo board

Hi Guys I'm Trying to find stm32l073rz Nucleo board datasheet that contains the boards pin description, but I can't find it anywhereI have found those but when I compare the pin description in the first pic from: NUCLEO-L073RZ | Mbedwith the one prov...

image.png image.png
Haystak by Associate II
  • 8271 Views
  • 15 replies
  • 9 kudos

Resolved! How to view the manual for HSE

Hello,I purchased a soldering crystal for X3 according to the BOM list,but it seems that the X4 on the board is the same product.Where is the X4 used?I checked UM2407 User Manual and STM32H742xI/G, STM32H743xI/G datasheets,but couldn't find it. Plus,...

HMsDobby2_0-1713509210530.png
HMsDobby2 by Associate III
  • 2409 Views
  • 1 replies
  • 2 kudos

Resolved! STLink v3 Not in Device Manager

Hello  I have been using an STLink v3 pod successfully for several months but suddenly it stopped working.  The green light is lit and the red one flashes slowly.  I cannot see it in Device Manager and there are no Unknown Devices.  There is no chime...

M_P by Associate II
  • 5926 Views
  • 8 replies
  • 0 kudos