STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H753ZI - PIN A2 - ADC

Hi,I'm using the H753ZI board with 26 ADC inputs on ADC1 & ADC3.The ADC pins run in DMA circular mode and all inputs seem to work fine except one pin: PA2PA2 is configured like the other pins: Analog mode, no pull-up and no pull-downBut the pin seems...

TVan8_0-1714667877397.png
TVan .8 by Associate III
  • 1787 Views
  • 2 replies
  • 0 kudos

Resolved! [Design review] STM32F0 custom board design

Hi everyone,I'm a beginner in electronics design but I'd like to create my own PCB.I've designed a schematic around the STM32F0 microcontroller and would greatly appreciate any feedback you might have.The setup involves a board with one transmitter a...

Tinou88_0-1714752030298.png
Tinou88 by Associate
  • 4294 Views
  • 4 replies
  • 2 kudos

STLINK-V3MINIE current draw

I am using a STLINK-V3MINIE  as a programmer with my custom board.The custom board has a battery holder, with 2xAA 1.5V each.A jumper is in series with the positive terminal of the battery holder, where I am using an ammeter.I measure a baseline of 3...

dhs by Senior
  • 1198 Views
  • 0 replies
  • 0 kudos

Finding JTAG/SWD location on custom PCB

Hey ST Community,A little bit of background knowledge. Aside from a few Arduino/microcontroller courses in college I am relatively new to coding and MCUs, specifically the ARM format. I currently work in the heavy machinery segment and am trouble sho...

20240502_094956.jpg 20240502_091123.jpg

Resolved! Using Timer Global Interrupt crashes board

I have an Arduino Giga (STM32H7). I'm trying to generate an interrupt on the Catch/Compare even of TIM5_CH3. TIM5 is set to one pulse mode and triggered as a slave to TIM1, they generate some PWMs; everything is working absolutely fine there. Also, I...

Pepijn by Associate II
  • 7845 Views
  • 11 replies
  • 1 kudos

Resolved! Does STlink support AD V2multi-drop SWD?

All STM32 CortexM7 and M33 have a ADI V2 debug unit. ADI V2 requires Multi-drop support, so that several SWD devices can be connected to SWD in parallel. Only with an activation sequence including the target-ID of that device to use selects the devi...

ILI9806 init DPI mode

Trying to make KD043WVFPA084-01-C015B LCD to work - custom board 32H735 chip. Display is from Startek that probably went under. Web page disappeared and no one answers emails. Display uses ILI9896E chip and as per data sheet it is setup for DPI mode ...

AS1956 by Associate II
  • 1429 Views
  • 1 replies
  • 0 kudos