Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, I have a board STM32F746G-DISCO from Farnell and I noticed that stm32cubeprogrammer is not showing the correct target board information. I have tried different version of stm32cubeprogrammer using different PC (2.15.0 due to usage of Windows...
Hi,I wanted to use an external voltage reference of +2.048V on the Nucleo Board. To do so I removed SB57 as dictated in UM1724 document: SB57 (VDDA/VREF+)ON VDDA/VREF+ on STM32 is connected to VDD.OFF VDDA/VREF+ on STM32 is not connected to VDD and c...
Hello everyoneI am using a Nucleo H7S3L8 evaluation module am I am trying to get some GPIOs and peripherals to work. I have generated a demo project that toggles a few LEDs and that works. Then I started replacing the GPIO ports (A, B, etc.) and pin ...
Dear STMicroelectronics Community,I am experiencing a critical issue with my NUCLEO-144 STM32N657X0 EVAL BRD following an attempted ST-LINK firmware upgrade.During the ST-LINK upgrade process (via STM32CubeProgrammer), the upgrade became stuck and di...
Excited to see a new connector on new STM32 Nucleo 144 boards like the Nucleo-H5E5ZJ. Is the Connector intended for customers to design their own modules only, or will ST offer a module as well? PS: I still hope to also see a Qwiic connector, or at...
I am currently using the NUCLEO-H563ZI board to test SPI functionality. I configured SPI1 as a master and was able to successfully transmit and receive data using HAL_SPI_TransmitReceive(). However, when I switched to SPI2, I found that the clock sig...
Hello!I just bought the stlink-v3minie for myself but I am unable to flash my board using it. I can program my board with a borrowed stlink-v3pwr but not with the minie.I have upgraded the firmware on it and it still doesnt work. It fails with this o...
Reference Board: Nucleo-H753ZI (MB1364, ST-LINK V3, rev B) Summary We have an external UART sensor (WitMotion HWT9053 IMU) connected to the Arduino D0/D1 header pins on a Nucleo-H753ZI. The sensor is confirmed working on Arduino. We have veri...
I realized that in my discovery board with STM32F411VE the accelerometer/magntometer is lsm303agr and not lsms303DLHC. I would have an updated schematic.