Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
quectel bg96 does not reply to messages from stm32l496ag on kit board p-l496g-cell02 but since I bought it. I could not even start blink the led on bg96 so I assume there is something missing to me. I use usb cable to stlink com and debug from the so...
Hi, I am using the STM32L4 B-L475E-IOT01A board with Wi-Fi module Inventek system ISM43362-M3G-L44.I have seen the example WiFi projects but they do not have the .ioc file. So my question is, is there any middleware available in STM32CubeMX which can...
I am experiencing issues powering the STM32H755ZIT6 MCU on our custom board. The schematic has been derived from the NUCLEO-H755ZI-Q development board reference design, and we have verified that there are no apparent design or assembly errors. Howeve...
Hi, I'm a beginner programming a NUCLEO-N657X0-Q. The LD5 is blinking and I can't get a connection to the board. Even with the demonstration code/project, it wouldn't work. In STM32CubeIDE I get the attached error message. As of yet, I never got to...
Split from Benchmark Validation in App does not match Arduino Uno R4 WiFi as this is a new question.thanks for the response @Andrew Neil If i'm not overstepping my bounds, given the requirements of an audio classifier (also need wifi support and disp...
Hello, I read somewhere that I can use the ST-LINK built into my H563ZI to program my custom cards with STM32F401.Could someone help me figure out how to do this?Thanks in advance.
Hello everyone, I'm facing a very frustrating issue with USART2 on my Nucleo-L475VGT6 board using the built-in ST-LINK Virtual COM Port. What works: - ST-LINK is detected (COM3 appears, Windows sound plays on connect) - Code downloads successfully (n...
iam attatching a pdf of my ki cad , let me know the what prevents to flash my code . this is the below error message coming while iam trying to flash " Starting server with the following options: Persistent Mode : Disabled Logging Level : 1 Listen Po...
Hello ST Community,I’m using an STLINK-V3MINIE and I’m trying to fully understand the hardware on the probe PCB.On the bottom side of the STLINK-V3MINIE PCB there is an unpopulated footprint labeled “CN5” (small pad footprint). I could not find any m...
Hi everyone, I recently bought an EVSPIN32F0602S1 board, but I’m unable to connect to it. Windows is giving me an error when I plug it in. I’ve already tried changing the USB cables and even tested it on different laptops, but I’m still gettin...