Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi ,Recently I got a NUCLEO-C051C8 board and tried to connect it to windows and program it using STm32CubeIDE but it does not show that st-link is connected , ST-link on board blinks RED continuously. Cant install it ( installation goes through , but...
Hi For some of my project, I need to measure the power consumption of the STM32N6570-DK while running a model on the CPU only versus an NPU + CPU accelerated workload. I am following the guide 1. How to measure power on the STM32N6 - STMicroele...
Hello All,I have the NUCLEO-C562RE board and I wanted to get started with it. But I am lost and not able to find any documentation related to architecture manual or user manual. I am new to ST boards, previously I used Aurix TC375. Has someone here i...
I have the following original debuggers:Stlink V2Stlink V3_SETStlink V3_MINIE (2 pieces)I was recently testing a simple board with an STM32U083 (powered by 3.3V) and found that two Stlink V3 MINIE units could connect to the MCU. Meanwhile, both the V...
How many uart channels are available on STM32H573I-DK Discovery kit.I am Looking for atleast two channels..Thanks in advance...
Hello, I am using an STM32F407VGT6 board with the ST-LINK debugger.When I plug the USB cable into the board, the LD1 LED on the ST-LINK stays Green and does not turn Red. From what I understand: Green LED indicates that ST-LINK is powered and idle. R...
Working with a NUCLEO-L552ZE-Q development board. Requirement is to interface this board to another larger board where all the pinouts on unpopulated footprints for CN11 and CN12 ( the "Morpho" connectors ) can be brought out. Therefore, the pos...
hi guys , I have been working on a stm32 project like a digital automotive cluster using STM32H7A3ViT6 MCU . I am using the LTDC module to drive the display . now the problem is the mcu dosent run the code on powerup but it ll do when i press the re...
Hello,I would like to build up an USB-CDC communication which gets the commands from the PC and forwards the messages to CAN. I have choosen a Nucleo-G431RB-C04 board, which have a FDCAN and a USB-FullSpeed inteface also. Do I able to create an USB-C...
Hi everyone,My company recently purchased a new ST-Link/v2 programmer. The problem is that after the firmware update, the device stopped working, and when I press the Connect button on the STM32CubeProgrammer, the following error appears:Error: ST-LI...