Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New STM32 VSCode extension V2.0.0 released

Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files)VS Code solution no longer r...

VSCode How to install VCPKG on VSCode with Zscaler/Proxy

Issue:  The VSCode don't have the ability to route the extension network requests to the proxy (only VSCode application network is routed to the proxy) I -  the clean way (applies to network with Zscaler installed) ask for a Zscaler power user profil...

NawresGHARBI_1-1704443433898.png NawresGHARBI_2-1704443503313.png NawresGHARBI_3-1704443553581.png NawresGHARBI_4-1704443616206.png

Hi, I am trying to generate sine modulated PWM on STM32F401-Disco board using MATLAB. The desired freq of a sine wave is 50Hz and of the carrier wave is 20kHz. But I am not getting 50Hz freq. Please suggest a solution.

I need sine modulated PWM during +ve half cycle of sine wave and zero output during -ve cycle of sine wave. Desired samples of sine are 200. I have attached the MATLAB simulation circuit snapshot. Problem is that I am getting 5Hz freq.

0690X000009jHLCQA2.png
VSira by Associate II
  • 181 Views
  • 3 replies
  • 0 kudos

Resolved! strange debugging behaviour

Hi,Im using the System Workbench and a strange behaviour occured to me.When a certain halting point is reached, Im not able to step to the next one. Pressing Resume brings me back to the very same halting point, stepping over aswell. And stepping int...

Anon767 by Associate II
  • 293 Views
  • 3 replies
  • 0 kudos

Snapshot mode in STMStudio

Hello! I trying to debug my application with STMStudio. In direct acquisition mode all working fine. But i can not find information about snapshot acquisition mode. Where i can find DataAcq.h and DataAcq.c? Or may be exist some example package?

SKole.17 by Associate II
  • 129 Views
  • 1 replies
  • 0 kudos

STM32072 configure error with Simulink

Dear all,I am trying to program STM32f072 microcontroller with simulink and i use Matlab R2013b and MAT Target 5.1.0 when i have used stm_config block to configure hardware target i got a problem that i can not set the block parameters.I herewith att...

KM.4 by Associate
  • 218 Views
  • 2 replies
  • 0 kudos