Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Need Help with Include paths in Keil compiler

Using Keil V5, C program for stm32g0. Have tried to add include paths in Project.Options for target. C tab. include paths, for instance:C:/Users/ashto/STM32Cube/Repository/STM32Cube_FW_G0_V1.6.1/Drivers/CMSIS/Include;..\..\STM32Cube\Repository\STM32C...

DRobe.4 by Senior
  • 1280 Views
  • 23 replies
  • 0 kudos

Resolved! Missing File STM32G070 on Keil

uVision V5.38.0.0 Trying to compile first program for STM32G0 and don't even get to the real compilation errors yet.Single file except for includes:#include "stm32g070xx.h"#include "stm32g0xx_hal.h"The warning and error are:ERNode_G070.c(61): warning...

DRobe.4 by Senior
  • 416 Views
  • 1 replies
  • 0 kudos

Debugging STM32G0

Hello, Currently I'm working on a system using the : STM32G0B1.I'm encountering some Hardfaults, for what I've seen on G0 finding the source of the hardfaults is complicated. I've used an code of type :typedef struct{ TByte rSHCSR_name[4]; TLongW...

0693W00000Ly0FKQAZ.png 0693W00000Ly0QIQAZ.png
Sego2 by Associate III
  • 436 Views
  • 4 replies
  • 0 kudos

Retarget printf for iar

In order to make the printf function accessible from other libraries, I create a retarget library where I call stdio and write my own implementation of _write function using UART peripheral. So when I want to use printf in another library. I add incl...

JCuna.1 by Senior
  • 270 Views
  • 1 replies
  • 0 kudos

I would to generate option byte file in hex format

@Exmple::020000041FFFDC:01F800000007:020000041FFFDC:01F80200FF06:020000041FFFDC:01F80400FF04:020000041FFFDC:01F80600FF02:020000041FFFDC:01F80800FF00:020000041FFFDC:01F80A00FFFE:020000041FFFDC:01F80C00FFFC:020000041FFFDC:01F80E00FFFA:00000001FFI was a...

Vikas1 by Associate
  • 314 Views
  • 3 replies
  • 0 kudos

Resolved! stm32g071rbIx or stm32g071rbTx?

I am using Keil Development environment for stm32g071 nucleo board. Which device should I choose? stm32g071rbIx or stm32g071rbTx? And how do I decide which one is correct for me?

Singh12 by Associate
  • 199 Views
  • 1 replies
  • 0 kudos