Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103C8T6 SPI

Hii all,First of all i am new to bluepill(stm32f103c8) and i want to use both the SPI1 & SPI2 for the same project .BUT i don't know how to use it i am using Arduino ide for code 

Kalp_13 by Associate
  • 224 Views
  • 1 replies
  • 0 kudos

Resolved! Read 96 bit UDID through serial bootloader or SWD

Hello,I am working on the STM32F103xx. I need to read out the 96 bit UDID (unique device ID) of the devices during production. Is there any way of reading this out from the serial bootloader on UART1 or through the SWD interface? I searched the AN315...

machinist by Associate III
  • 593 Views
  • 5 replies
  • 0 kudos

Build the code for Keil

I configured lwip in cube for stm32f107, when I generate code for keil and run it the micro hangs, but if I write a program without cube, it runs without any problem.What is the problem?Note: If I get the output for CubeIDE, it runs without any probl...

HKabi.1 by Associate II
  • 1002 Views
  • 11 replies
  • 1 kudos

CAN Bus between STM32F103 and Arduino

I have a few arduino boards communicating through each other on a CAN Bus. Arduino is connected to a MCP2515 CAN Bus Module TJA1050.All arduino are communicating properly between each other. Here is an example of my reader on arduino:#include "MIDIUS...

Is it a problem to use TIM1 PWM ch1..3 under Arduino?

Dear reader,I have a question about the use of TIM1 on the Blue Pill STM32F103. I want to build a synchronous Buck Converter using the Blue Pill and need to use PWM on TIM1 ch1..3 with its complementary outputs and the programmable dead time for that...

WOGoos by Associate II
  • 352 Views
  • 3 replies
  • 0 kudos

Resolved! Arduino milis() function stm32f103xx

I am trying to port some Arduino library to stm32. In Arduino, millis() returns the number of milliseconds since boot. Is there an equivalent function in stm32? I am using stm32f103 MCU.

Bicer by Associate II
  • 1811 Views
  • 6 replies
  • 1 kudos