I am just getting one error and it dosent seem to go.Can anyone help me to figure out why this error is coming and help me to resolve it asap.I have attached a screenshot of the same for the refrence below.
I would compile the firmware STM32072 for the STM32L152 Discovery with TrueStudio. Ihave got the fatal error: tsl_acq_stm32l1xx_sw.h: No such file or directory
We've got some piece of code that we would like to debug on the MCU. This works fine with the previous hardware version of our product, which uses an STM32L151RET6.On our new hardware version using the STM32L151VE, however, debugging from IAR does no...
Hi I am using STM32L151RBT6 controller card. This was working properly also there was no issue in debugging. I am using IAR Embedded Workbench 6.4.I Added this line to my code: FnEraseEpromWord(0x080800F5,1); as because I want to erase data for this ...
Hello. Today when I was programming my STM32L151CBU6A on System Workbench I get a message like this when trying to release or debug. In STLINK I find option bytes and uncheck protected areas but it doesn't help. Still the same issue. I can normall pr...
Hi,there is a bug in newest STMB Cube with newest Firmware and STM32L151CCT.Cube Version is 5.2.0, FreeRTOS V10.0.1.I had a project with older Firmware which was imported from other project and I set the Memory usage to Static. I get an error in heap...
I'm working with the STM32L152RE, which has dual flash banks. Each bank has a binary file image loaded. I'm trying to start the debugger in Bank 1 (0x08000000), have it stop at main() (or some specific address) and debug in assembly. I haven't been a...
Posted on May 24, 2017 at 11:06The last driver for L1, version 1.7.0 contains this error when trying to compile projects in OpenSTM32 IDE where I replaced the HAL driver by hand. So I had to revert to 1.6.0 version. stm32l1xx_hal_rtc.c:424:38: error...
Posted on July 17, 2015 at 12:08Hi,I started for IAP with stm32 using iDE KEIL which works fine.But now when i switch to iDE IAR using STM32F101VCT6 the IAP not working,for switching from one code to another code written in the flash memory space.Fo...