Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Need Help with Include paths in Keil compiler

Using Keil V5, C program for stm32g0. Have tried to add include paths in Project.Options for target. C tab. include paths, for instance:C:/Users/ashto/STM32Cube/Repository/STM32Cube_FW_G0_V1.6.1/Drivers/CMSIS/Include;..\..\STM32Cube\Repository\STM32C...

DRobe.4 by Senior
  • 1158 Views
  • 23 replies
  • 0 kudos

how to solve this error? in simulink

Hi.i uses matlab2019 and i want to design software using simulink.but, when i add "GPIO_WRITE STM32", simulink generates this error. did you know about this error? and solution?

0693W000008wDwQQAU.png
IB1 by Associate
  • 225 Views
  • 1 replies
  • 0 kudos

Resolved! Exception return value 0xffff fff9 on stack?

When debugging start-up problems, I've found this stack in TrueSTUDIO: According to the Programming Manual, an exception return value of 0xffff fff9 denotes "Return to Thread mode, exception return uses non-floating-point state from MSP and execution...

0693W000007BYTHQA4.png

Resolved! The reset value of GPIOB register of STM32F401RCT6

When I simulate STM32401RCT6 with IAR,the MCU is on reset state;IAR shows the value of GPIOB register :ODR=0x00000280;but refer to the reference manual ,the reset value of GPIOx_ODR=0x00000000.Did I do something wrong when simulated?Thanks very much...

0693W000003RfuzQAC.png 0693W000003RfuBQAS.png
Pzhu.1 by Associate II
  • 254 Views
  • 1 replies
  • 0 kudos

Resolved! Problem with step one opening example file?

Carefully following the instructions I got with my STM32 Nucleo board I am trying to opent the: C:\Users\myname\STM32Cube\Repository\STM32Cube _FW_L4_V1.11.0\Projects\NUCLEOL476RG\Examples_LL\ GPIO\GPIO_InfiniteLedTogglingThen project:GPIO_InfiniteLe...

0693W000001tTMAQA2.jpg
WBerr.2 by Associate
  • 372 Views
  • 3 replies
  • 0 kudos