Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Keil Trace Exceptions

As shown below the screen, when I am running the MCU application, it is running without any flaws. However, when I notice the TraceExceptions window on Keil IDE, noticed a large number of hard faults occurring. But these faults do not trigger fault h...

0693W00000GYHooQAH.png
KSing.4 by Associate II
  • 198 Views
  • 0 replies
  • 0 kudos

Licence terms SW4STM32

Posted on September 06, 2017 at 12:19I just want to know if the code / std peripheral Libraries generated by STM32cube for STM32F411 and for IDE AC6, can be used for commercial products(sell products) ? #std_lib #sw4stm32 #stm32f4 #stm32 #licence #s...

error an entity with internal linkage cannot be referenced within an inline function with external linkage (after using SPL2LL Convertor)

Posted on July 21, 2017 at 17:25Hello ,  after using the SPL2LL convertor to migrate from lib STD to libLL ,i compile my project so i have this error ' an entity with internal linkage cannot be referenced within an inline function with external link...