Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New STM32 VSCode extension V2.0.0 released

Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files)VS Code solution no longer r...

VSCode How to install VCPKG on VSCode with Zscaler/Proxy

Issue:  The VSCode don't have the ability to route the extension network requests to the proxy (only VSCode application network is routed to the proxy) I -  the clean way (applies to network with Zscaler installed) ask for a Zscaler power user profil...

NawresGHARBI_1-1704443433898.png NawresGHARBI_2-1704443503313.png NawresGHARBI_3-1704443553581.png NawresGHARBI_4-1704443616206.png

STM32C031-KEIL-breakpoint

STM32C031 is simulated in KEIL, but only a few breakpoints can be added during the running process, and the level is also level0.How to locate this kind of problem,Thank you very much for your help!

Arduino UNO R3 with the x-nucleo-iks01a3

Hi, i connected the Arduino UNO R3 with the motion MEMS and environmental sensor evaluation board system: X-NUCLEO-IKS01A3 of ST. I installed the library (STM32duino,LSM6DSO), and tried to create a code for a self-balancing robot. But it doesn't prin...

Giuseppe1 by Associate III
  • 274 Views
  • 3 replies
  • 0 kudos

Recovering MCU from read out protection level set to 0xFF

Dear allI’m not able to reset RDP to level 0Custom board with STM32F732ZET6Not sure, but something goes wrong and I think the information block was erased only – without programming afterwards“The value of an option is automatically modified by first...

FWege.1 by Associate III
  • 444 Views
  • 7 replies
  • 0 kudos

SPI communication while debuging

Hi,I using STM32F407IG in IAR Embedded workbench.When I debug the program the SPI communication does not work.what could be the reason?Without debug the SPI work

Aldo1 by Associate II
  • 654 Views
  • 15 replies
  • 1 kudos

Resolved! Conversion DFU-File to Hex-File

I try to convert a DFU-File to a Hex-File with the ST-Tool  "DfuFileMgr.exe" from the DfuSe_v3.0.6 Toolkit.The reason for the conversion is, that we have an Update-Application in the field that works with USP-DFU update and the old DfuSe driver. Now ...

urban17 by Associate
  • 1318 Views
  • 3 replies
  • 1 kudos

hal_stm32 on Zephyr 3.2.0

Hi everyone. I'm currently working on a legacy project that only runs on Zephyr V3.2.0. I have to use the hal_stm32 to get some peripherals running (https://github.com/zephyrproject-rtos/hal_stm32). The latest version of hal_stm32 is not compatible w...