Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 extension for vscode is not working.

Greetings, I'm trying to set up Visual Studio Code to work with STM32 microcontrollers. I've installed the STM32 VS Code Extension, as well as CubeCLT, CubeMX, and FINDER as requested, all with the correct versions to ensure functionality. I've also ...

luxae by Visitor
  • 15 Views
  • 0 replies
  • 0 kudos

STM32 VS Code Extension and Devcontainer

I am a happy VSCode developer using docker devcontainers to create an easily reproducible environment for development. I am struggling with a strange bug with the "STM32 VS Code Extension" (v2.0.1).If I try to access it, after opening the container, ...

pcb by Associate
  • 287 Views
  • 1 replies
  • 1 kudos

VSCode extension build and only flash program

I started using stm32 MCU's on my university. There we used the CubeIDE. Now I have a board at home for own projects. I wanted to use VSCode with the new extension, because i prefer it over Eclipse / CubeIDE. Now I have two questions. I can debug my ...

maze2go by Associate
  • 2489 Views
  • 9 replies
  • 4 kudos

New STM32 VSCode extension V2.0.0 released

Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files)VS Code solution no longer r...

Resolved! Start debugging STM32 VS Code Extension

I was using the SystemWorkbench for years and everything OK.  Recently changed to STM32CubeIDE and also able to build and debug within hours with released ST project "STM32Cube_FW_F4_V1.28.0".Have tried to use the new "STM32 VS Code Extension" in VSC...

DilbertK_0-1709248326176.png

Resolved! Need help with VScode + cmsis arm_math.h

Hi Guys, I'm new about VScode. I try to use arm_math.h in my program. but after i set include path in json file, the vscode can't find the function. and give me the message <<Function definition for 'arm_mat_init_f32' not found.C/C++>> my board is nu...

Leon_D by Associate II
  • 525 Views
  • 5 replies
  • 1 kudos