Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hello, I am using stm while controlling a device and after working conditions for a while, I saw that the software made itself like this. I have not encountered it on other devices. When I put the software on the processor again,it gets fixed,what reason?

That is part of broken softwareD8 0A 00 20 CD 02 00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ...

0693W00000Lz1QVQAZ.png

Resolved! STM32H750VBT6 & CubeMX & IAR

Hi everyone ;I am having a strange issue with IAR . I configured the mcu via cubemx and generated it then I build all the files but I got the errors in the attached files when I try to download the code into the MCU . But I don't get any issuse with...

BG1 by Senior
  • 541 Views
  • 7 replies
  • 0 kudos

What special requirements does ST-LINK_gdbserver place on an external flash loader? My loader works with ST-Link Utility, STM32CubeProgrammer, but not ST-LINK_gdbserver.

I've written an External Flash Loader and successfully tested erase, read, and write functionality first in my own firmware, then with ST-Link Utility v4.5.0, and also with STMCubeProgrammer v2.6.0.However, when I try to use it to debug with TrueStud...

Flash Loader Demo could not work with the STM32ML4xx

When I used the Flash Loader Demo to connect with the STM32L412, it could not connect successfully. I checked the AN2606, it said the MCU will reply two ack (0x79) this is different than others. I guess this should be the problem to block the connect...

Haifeng by Associate II
  • 207 Views
  • 1 replies
  • 0 kudos