Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

power consumption stm32l4 in lprun mode

HiI am using stm32l496 in lprun mode but the current consumption is equal to 1.2 mA while in run mode the current consumption is equal to 3 mA while in the datasheet, the current consumption in the lprun mode is about 220 uA.how can I reduce the curr...

0693W00000FAPmAQAX.jpg
alianvari by Associate III
  • 2442 Views
  • 2 replies
  • 0 kudos

Hi, I am trying to test Low power Sleep mode on Nucleo-4R5ZI development board. Unfortunately i am getting following errors and not entering into sleep mode and not working Debug mode.

Please help how can i test low power modes on development Nucleo-4R5ZI board. I am working AC6 tool and used the path STM32Cube_FW_L4_V1.13.0\Projects\NUCLEO-L4R5ZI\Examples\PWR\PWR_LPSLEEPand got the below errorsInfo : Previous state query failed, t...

MBhar by Associate II
  • 150 Views
  • 0 replies
  • 0 kudos