Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103C8T6 RTC losing date

Hi, I am working on a simple datalogger project using the STM32F103C8T6, I am currently using the STM32RTC library to access the RTC peripheral via a custom-built board. I originally prototyped using Blue Pill but quickly migrated away from that once...

PDack.1 by Associate
  • 303 Views
  • 0 replies
  • 0 kudos

STM32F4 Discovery Board Control Register Problem

I open an empty project without any settings.#include "stm32f4xx.h" #include "stm32f4_discovery.h"   int main(void) { while (1) {   } }   void EVAL_AUDIO_TransferComplete_CallBack(uint32_t pBuffer, uint32_t Size){ /* TODO, implement your code...

0690X000009Xg3JQAS.png
vortex by Associate
  • 123 Views
  • 0 replies
  • 0 kudos

Resolved! clock frequency calculations

Hi,I am going to use internal osc for generating a frequency of signal 36khz. Do i need any external circuitry for it ..?For selection of 8Mhz frequency as clock can it be done in cube mx only and generate a source code form there...?Selection of pr...

HSE can not be ready at debug

Posted on July 09, 2013 at 09:34 In mySetSysClockTo72 function, there is /* Wait till HSE is ready and if Time out is reached exit */ do { HSEStatus = RCC->CR & RCC_CR_HSERDY; StartUpCounter++; } while((HSEStatus == 0) && (Star...

auzgec by Associate II
  • 671 Views
  • 9 replies
  • 0 kudos