Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Upload .bin files on windowsthrough the USB interface

Hi, I just decided to try mbed OS 6 for programming my NUCLEO-WB15CC. Compilation is successful, but when i try to flash the compiled .bin file, the operation fails saying that a device was not connected even though it was. I am guessing it is becaus...

Elijah1 by Associate
  • 634 Views
  • 0 replies
  • 0 kudos

Problems using ST-GDB Server on Linux Mint

I have the newest Version of ST/Atollic TrueStudio installed on my Linux Mint Machine. Operating System: Linux Mint 19 Kernel: Linux 4.15.0-20-generic Architecture: x86-64When Itry to upload my Code I get the following error:STMicr...

PWass by Associate
  • 248 Views
  • 1 replies
  • 0 kudos

Resolved! How to change ST-LINK settings in SW4STM32 IDE

Hello,I have a probably simple question: Where I can change ST-LINK Settings in System Workbench IDE. For example in ST-LINK Utility in Settings I can change Reset Mode to Software System Reset,and I don't know where I can find this setting in IDE.I ...

0693W000000UtjVQAS.png 0693W000000UtkdQAC.png
DKarc by Associate II
  • 677 Views
  • 2 replies
  • 0 kudos

OpenOCD support for external STLink debugger

Posted on November 05, 2017 at 07:41Hi all,Is anyone using OpenOCD with genuine external STLinkV2 debugger/programmer and STM32L0? Clearly, there is an issue as I have tested multiple units and OpenOCD releases (0.9, 0.10.).The debuggers are fully f...