Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with Single Step STMF7

Posted on December 07, 2016 at 21:47 There is a problem with IDE debuggers for STMF7, and as I understand, all ARM M7 core based processors. With other CORTEX controllers, when a debbuger pauses or hits a breakpoint, the debugger stops interrupt pr...

Debugging, but not running.

Hey,I build my own STM32 board with the STM32L011G3 and started testing with a simple blinking program via SWD and ST-Link V2.  When I'm debugging it, everything works fine, but when I use the run command in SW4STM32 the LED lights up, but does not t...

Resolved! Compare ONLINE<->OFFLINE project

Dear experts,I am new to STM32 world, so I apologize, if my question is inappropriate.Is there a way how can I see the program differences between saved project (PC) and the one that is loaded in the MCU?I'm using System Workbench IDE to program stm...

MBirz.1 by Associate
  • 266 Views
  • 2 replies
  • 0 kudos

Resolved! Problem importing from STM32CubeMX to System Workbench

Posted on May 07, 2018 at 04:00I have been importing CubeMX projects into System Workbench (SW4STM32). It's been working great, a real time saver. I first open System Workbench and select a workspace. Then using CubeMX I configure the project and ge...

How to include a STM32L451xx project on Jenkins?

Hi, Am using the SW4STM32 on Win 10 to develop an IoT project witha STM32L451xx device (included FreeRTOS and CMSIS on the project). I would like to integrate this project into Jenkins so that I can automate the build and testing processes. I would b...

Ivera by Associate
  • 186 Views
  • 0 replies
  • 0 kudos