Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error Writing 64 bit in FLASH

Tranferring data from serial input,(in my case idDA), or from an SD, may be you try to write a double word a time (64bit) in flash area and you may use the:HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, flash_ptr,codeData64). This function calls th...

Regarding STM32F4 Micro Controller

Hello Folk,Am working on STM32f4 Micro-Controller,Earlier I Checked Micro Controller with St Utility there i Observed Flash Size and Revision Id of Micro Controller Not Showing (Unknown) so I Doubted on Fake Micro Controller, and i Went through the M...

AGond.2 by Associate III
  • 423 Views
  • 3 replies
  • 1 kudos

Mass Erase to unlock the device

Hello, I Have few Query Related to Flashing.In newly Arrived Board am doing first time code Flashing from IAR tool with the help of JTAG Debugger.so First Message Pop Up like Perform Mass Erase to unlock the Device Press okay.After Doing Sud...

AGond.2 by Associate III
  • 377 Views
  • 0 replies
  • 0 kudos

STM32F407VGT6U (DISC1) External mode : Could not connect to target application: XCP internal error: timeout expired, in response to XCP CONNECT command

Hello guys!I'm trying to use external mode with STM32F407VGT6U(older version of this discovery board) and Embedded Coder Support Package for STMicroelectronics STM32 Processors, I'm running on Matlab r2023a with all the support packages freshly insta...

GDan.2 by Associate
  • 518 Views
  • 0 replies
  • 2 kudos