Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK V2 Update error Unexpected flash size

Used this ST-Link V2 with W10 some years ago. Now on Linux I want to use it with openocd and got error:ST-Link version does not support DAP direct transportMost likely the cable adapter needs update.But the STLinkUpgrade.jar reported  Unexpected flas...

Commercial use

Hello, Can the following licenses be used free of charge by a company for commercial purposes? Cube IDE https://www.st.com/en/development-tools/stm32cubeide.html   Cube Mx https://www.st.com/en/development-tools/stm32cubemx.html   CubeProg https://ww...

STM32CubeMonitor-Power window stuck and will not close

After some time I found the tool displaying an error of sort, I think something regarding inactivity.Following that I can't close the sampling window. I can't move it or minimize it , or press any button in its GUI.  All buttons are unresponsive.I ca...

DS.4 by Senior II
  • 729 Views
  • 2 replies
  • 1 kudos

Resolved! Cannot download STM32CubeCLT

I am logged into my STM user account.I get to the download page for STM32CubeCLT (https://www.st.com/en/development-tools/stm32cubeclt.html#get-software) and I try to download the latest version for Windows.A dialog pops up with 'Log in to MyST', 'Cr...

MWils.4 by Associate II
  • 650 Views
  • 3 replies
  • 0 kudos

Arduino UNO R3 with the x-nucleo-iks01a3

Hi, i connected the Arduino UNO R3 with the motion MEMS and environmental sensor evaluation board system: X-NUCLEO-IKS01A3 of ST. I installed the library (STM32duino,LSM6DSO), and tried to create a code for a self-balancing robot. But it doesn't prin...

Giuseppe1 by Associate III
  • 276 Views
  • 3 replies
  • 0 kudos

Recovering MCU from read out protection level set to 0xFF

Dear allI’m not able to reset RDP to level 0Custom board with STM32F732ZET6Not sure, but something goes wrong and I think the information block was erased only – without programming afterwards“The value of an option is automatically modified by first...

FWege.1 by Associate III
  • 445 Views
  • 7 replies
  • 0 kudos

Resolved! Conversion DFU-File to Hex-File

I try to convert a DFU-File to a Hex-File with the ST-Tool  "DfuFileMgr.exe" from the DfuSe_v3.0.6 Toolkit.The reason for the conversion is, that we have an Update-Application in the field that works with USP-DFU update and the old DfuSe driver. Now ...

urban17 by Associate
  • 1324 Views
  • 3 replies
  • 1 kudos